Hi NXP expert,
I would like to know whether CBTU02044 support hot plug, could you please help to confirm ? I found the following description in the datasheet.
"Back current protection on all I/O pins of these switches"
Solved! Go to Solution.
Hi
A host system which supports hot plug can/should detect an endpoint/device plugging/adding to it, and support the device (with power, status update, etc.), without having to turn off /reset system power.
Hot-plug is a system function, I don’t think it is relevant to the MUX, because CBTU02044 doesn’t do detection, no register, no interrupt pinout……
The system can switch the MUX channel to connect to new endpoint/device without reset the power.
Hi
A host system which supports hot plug can/should detect an endpoint/device plugging/adding to it, and support the device (with power, status update, etc.), without having to turn off /reset system power.
Hot-plug is a system function, I don’t think it is relevant to the MUX, because CBTU02044 doesn’t do detection, no register, no interrupt pinout……
The system can switch the MUX channel to connect to new endpoint/device without reset the power.