Difference between PCF8563T/F4,112 and PCF8563T/F4,118?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between PCF8563T/F4,112 and PCF8563T/F4,118?

1,777件の閲覧回数
Cryptonite
Contributor I

We have been PCF8563T,112 for a number of years but are now told it's no longer available and offered PCF8563T/F4,118 instead. The datasheets for the two parts are identical (Rev. 11 - 26 October 2015) and there is no mention of the suffixes in it.

Can anyone tell me what, if any, the differences are between the 112 and the 118 parts are, please?

0 件の賞賛
返信
1 返信

1,755件の閲覧回数
nxf45548
NXP Employee
NXP Employee

Hi Steve, 

The difference is the packing type. 118 makes reference to REEL-Reel 13" Q1/T1 and 112 to TUBE NDP DSC BULK PACK 
You can check the following link for more reference about packing:
https://www.nxp.com/docs/en/supporting-information/Packing_Letter_code.pdf


0 件の賞賛
返信