Using 8 ohm speakers with TDF85xx.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using 8 ohm speakers with TDF85xx.

886 Views
wgchae
Contributor I

Hi,

I'm looking for a class-D audio amplifier with speaker diagnostics.

I'm checking TDF8530TH/N2, TDF8597TH/N1, TDF8599CTH/N1.

1. We use 8 ohm speakers but the data sheet contains only the specifications for the 4 ohm and 2 ohm speakers.

  I would like to know the following specifications for 8 ohm speakers.

- Recommended supply voltage.

- Max output.

- Output(W) to THD+N graph (according to audio frequency).

  Specification of our device : THD+N is less than 3% when 1kHz audio, 20W output condition.

                                               The output power difference between 200Hz(5kHz) and 1kHz should be within +-5dB.

2. Can I manually run DC diagnostics after the IC is powered on?

   If possible, please let me know the sequence of S/W processing.

Thanks.

Woo-Geun.

0 Kudos
2 Replies

768 Views
m-bab
Contributor I

Dear TechSupport,

I am also looking for a configurable low-power class-D audio amplifier (with I2S). I also found the two named ICs very interesting (TFA9879, TFA8200) - but on both product pages the statement "not recommended for new designs" can be found. Why is that and does it really affect both products? Is the whole category of digital low-power audio amplfiers abandoned at NXP?

Kind regards,
Martin

0 Kudos

833 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

For 8 ohm speaker applications I would rather recommend you to take a look at the following devices: 

  1. TFA9879 “Mono BTL class-D audio amplifier for portable applications with digital input”: https://www.nxp.com/docs/en/data-sheet/TFA9879.pdf

 

  1. TFA8200 “Mono BTL class-D audio amplifier with digital inputs for IOT applications”: https://www.nxp.com/docs/en/data-sheet/TFA8200.pdf

 

I hope one of these devices can be useful for your application.

Regards,

Jose

0 Kudos