DSP 56F8367 external memory access

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DSP 56F8367 external memory access

2,408 次查看
technicalquesti
Contributor I
Hi,
I can't understand, can I use all 20-bit of external address bus for external Data memory if I use in my design Mode 0(MA=0) and EX=0 for OMR register. I'd like to use internal Program flash memory and external Data memory about 256K.
标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,154 次查看
marvin
Contributor I
Hi,

There shouldn't be a problem to use extended addresses in the internal boot, but you need to configure address lines A17-Axx yourself. They are configured as a GPIO after reset in this mode (MA=0). The best way is to use ProcessorExpert tool for configuration. The CPU bean provides settings of the external bus and PE can help you very well.
0 项奖励
回复