DSP 56F8367 external memory access

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSP 56F8367 external memory access

2,308件の閲覧回数
technicalquesti
Contributor I
Hi,
I can't understand, can I use all 20-bit of external address bus for external Data memory if I use in my design Mode 0(MA=0) and EX=0 for OMR register. I'd like to use internal Program flash memory and external Data memory about 256K.
ラベル(1)
  • DSC

タグ(2)
0 件の賞賛
返信
1 返信

1,054件の閲覧回数
marvin
Contributor I
Hi,

There shouldn't be a problem to use extended addresses in the internal boot, but you need to configure address lines A17-Axx yourself. They are configured as a GPIO after reset in this mode (MA=0). The best way is to use ProcessorExpert tool for configuration. The CPU bean provides settings of the external bus and PE can help you very well.
0 件の賞賛
返信