Compiling the AXE Package with the LTIB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiling the AXE Package with the LTIB

ソリューションへジャンプ
3,031件の閲覧回数
adelcinque
Contributor I
Hi all,
I'd like to create and run a task on the MPC5121e AXE processor for performance testing. On the ADS5121 BSP docs I found:

"To compile the axe package you need to copy the axe_scheduler package AXE_SCH_1_0_5_P1.zip and the axe codec binary package axe_codecs_linux_20080219_bins.tar.gz into /opt/freescale/pkgs"

but i could not find these files in the BSP, nor on the gpp. Is there any other place I should check?

Also, it seems I need CodeWarrior to build code for the AXE processor. Isn't there a toolchain and HOWTO available for building without CW? I could not register CW (it seems my product key is not accepted anymore!)

Thanks
0 件の賞賛
返信
1 解決策
1,983件の閲覧回数
fsl_linux_spt
Contributor III
sorry this was not replied to earlier.  It was determined that the AXE package mentioned in the doc have propriatary restrictions so they were not made available in the bsp.  The status of these pacakges are still not publicly available. 
 
 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,984件の閲覧回数
fsl_linux_spt
Contributor III
sorry this was not replied to earlier.  It was determined that the AXE package mentioned in the doc have propriatary restrictions so they were not made available in the bsp.  The status of these pacakges are still not publicly available. 
 
 
0 件の賞賛
返信