Can AFT05ms003n can work with adrain supply of 3.3V for producing an output of 24dBm?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can AFT05ms003n can work with adrain supply of 3.3V for producing an output of 24dBm?

759 Views
rekha1
Contributor I

Hi,

I would like to know whether AFT05ms003n can be used to produce an output of 24dBm with a drain supply of 3.3V. What should be the gate bias? Is there any reference document or design?

Labels (1)
  • RF

Tags (1)
0 Kudos
4 Replies

619 Views
LPP
NXP Employee
NXP Employee

Yes. It is possible.

ADS load pull simulation provides typical P1dB=25dBm, Gain=15dB, PAE=59% @ 100MHz


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

619 Views
rekha1
Contributor I

Thank you so much LPP.

 

1. Can you please share the circuit used for this simulation?

2. Which was the platform used for simulation of the same?

 

Thank you  in advance for any help you provide

 

Rekha K

SRF

Cetronics technologies

0 Kudos

619 Views
LPP
NXP Employee
NXP Employee

I used Keysight ADS load-pull design guide framework. Snapshot is attached.

In addition, the circuit provides stability enhancement: R1 for high frequency, SRC1 feedback for low frequency.


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

619 Views
rekha1
Contributor I

Thank you so much LPP.

1. Can you please share the circuit used for this simulation?

2. Which was the platform used for simulation of the same?

Thank you  in advance for any help you provide

Rekha K

0 Kudos