Boot the lx2160ardb_rev2 in sdcard mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot the lx2160ardb_rev2 in sdcard mode

463 Views
Jayalakshmi24
Contributor I

Hi

My task is to boot the lx2160ardb_rev2 in sd card mode and to create partition with the binaries.How to disable other .dtb except lx2160ardb_rev2 from the generated boot_LS_arm64_lts_5.10_202405091415.tgz?

Labels (1)
0 Kudos
Reply
3 Replies

411 Views
LFGP
NXP TechSupport
NXP TechSupport

Actually is not possible to generate only one .dtb file as you want

0 Kudos
Reply

403 Views
Jayalakshmi24
Contributor I

Hi 

Thanks for the reply. I need only dtb files which is related to lx2160ardb_rev2.

0 Kudos
Reply

387 Views
LFGP
NXP TechSupport
NXP TechSupport
please run the next command in order to get the dbt file among other needed file, the command will generate a tarball,
$ bitbake generate-boottgz
review into the LLDP user manual the chapter "3.5.6 Generate tarball"
0 Kudos
Reply