A5G07H800W19NR3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A5G07H800W19NR3

275件の閲覧回数
Joey-Community
Contributor I

Dear NXP

Do you know the difference between dissipasion power and saturated power?

And what is the dissipasion power for below part?

NXPA5G07H800W19NR3
NXPA5G21H605W19NR3
NXPA5G18H610W19NR3
NXPA5G19H605W19NR3
NXPA5G08H800W19NR3
0 件の賞賛
返信
1 返信

252件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

The Saturation power (Psat) is the power level achieved, even changing the input power does not produce any change in the output power level.

The dissipation power is  is the maximum allowed continuous power dissipation for a device with a mounting base at 25 C. The power dissipation is calculated as that which would take the device to the maximum allowed junction temperature while keeping the mounting base at 25 C.

The maximum rating for power dissipation (PD) is closely associated with thermal resistance (θJC). Actually maximum PD is in reality a fictitious number a kind of figure of merit because it is based on the assumption that case temperature is maintained at 25°C.

Hope this helps.

0 件の賞賛
返信