9S08QE128 baud rate to 115200?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9S08QE128 baud rate to 115200?

ソリューションへジャンプ
607件の閲覧回数
GaryOlmstead
Senior Contributor I

Hi --

I am using a 9S08QE128, (internal clock oscillator, FEI mode), and have to tie it to a Bluetooth module that has a fixed baud rate of 115200.  I can get there with the QE128 by setting the internal oscillator to 36kHz, bus freq divide by 1, internal bus clock to 9.216MHz, and setting the DCO mode to "default 512", instead of "fine tuned 32kHz".

My question is, what does not selecting fine tuned mode do to the oscillator accuracy?  The data sheet talks about "user trimmed" reference frequency, but we don't really have the resources to do that in production quantities.  What is the accuracy if I use it as it comes from the factory?

Gary Olmstead

Ventura CA

0 件の賞賛
返信
1 解決策
574件の閲覧回数
GaryOlmstead
Senior Contributor I

I found the answer.  If anyone else has this problem, AN2496 explains all.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
575件の閲覧回数
GaryOlmstead
Senior Contributor I

I found the answer.  If anyone else has this problem, AN2496 explains all.

0 件の賞賛
返信