How can i generate an user certificate of A1006?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i generate an user certificate of A1006?

663 Views
aoboyan
Contributor I

I want to generate an user certificate of A1006 writting into A1006. Through reading relavant manuals, i discovered that there are tool of The A100x Customer Provisioning Utility to make it, but the example show the needs of smart cards, is it right? What if i want to do it? some tools?

0 Kudos
Reply
3 Replies

583 Views
Kan_Li
NXP TechSupport
NXP TechSupport

As far as I know, the option of smart card is not available now. NXP writes the certification data into the chips and ships them to you.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

583 Views
aoboyan
Contributor I

what tool or software do i need to what i want to generate a usr_certificate? Customer Provisioning Utility?

0 Kudos
Reply

583 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Please consider that the information regarding the A1006 is under NDA, if you are already working with the device and have the information of it from DocStore  you can see that there is an application note with information of the certificate injection options for customers. 

Regards,
Estephania

0 Kudos
Reply