56f8323 - SPI, how can i drive the SS1 Pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

56f8323 - SPI, how can i drive the SS1 Pin

ソリューションへジャンプ
1,915件の閲覧回数
Kai
Contributor I
Hello,    i want to use a seriell flash memory from st at a 56f8323. How can i toggle the SS1 pin? I want to use this pin for CS. Or must i use a GPIO pin for CS?
Thanks
Michael
Alban Edit: FSL Part Number in Subject line.

Message Edited by Alban on 2007-03-15 06:45 PM

ラベル(1)
  • DSC

0 件の賞賛
1 解決策
961件の閲覧回数
admin
Specialist II
As far as I understand SS pin in this MCU may be configured as input or it state ignored at all. So configure this pin as GPIO output.

元の投稿で解決策を見る

0 件の賞賛
1 返信
962件の閲覧回数
admin
Specialist II
As far as I understand SS pin in this MCU may be configured as input or it state ignored at all. So configure this pin as GPIO output.
0 件の賞賛