56f8323 - SPI, how can i drive the SS1 Pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

56f8323 - SPI, how can i drive the SS1 Pin

Jump to solution
1,990 Views
Kai
Contributor I
Hello,    i want to use a seriell flash memory from st at a 56f8323. How can i toggle the SS1 pin? I want to use this pin for CS. Or must i use a GPIO pin for CS?
Thanks
Michael
Alban Edit: FSL Part Number in Subject line.

Message Edited by Alban on 2007-03-15 06:45 PM

Labels (1)
0 Kudos
Reply
1 Solution
1,036 Views
admin
Specialist II
As far as I understand SS pin in this MCU may be configured as input or it state ignored at all. So configure this pin as GPIO output.

View solution in original post

0 Kudos
Reply
1 Reply
1,037 Views
admin
Specialist II
As far as I understand SS pin in this MCU may be configured as input or it state ignored at all. So configure this pin as GPIO output.
0 Kudos
Reply