56f8323 - SPI, how can i drive the SS1 Pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

56f8323 - SPI, how can i drive the SS1 Pin

跳至解决方案
1,952 次查看
Kai
Contributor I
Hello,    i want to use a seriell flash memory from st at a 56f8323. How can i toggle the SS1 pin? I want to use this pin for CS. Or must i use a GPIO pin for CS?
Thanks
Michael
Alban Edit: FSL Part Number in Subject line.

Message Edited by Alban on 2007-03-15 06:45 PM

标签 (1)
0 项奖励
回复
1 解答
998 次查看
admin
Specialist II
As far as I understand SS pin in this MCU may be configured as input or it state ignored at all. So configure this pin as GPIO output.

在原帖中查看解决方案

0 项奖励
回复
1 回复
999 次查看
admin
Specialist II
As far as I understand SS pin in this MCU may be configured as input or it state ignored at all. So configure this pin as GPIO output.
0 项奖励
回复