I am not sure if I am posting this in the correct place or not, because I am not sure if the problem lies in codewarrior itself, however, I will give it a shot.
I have have defined 2 arrays in which I want to store the results from two different ADC result registers.
If I try to write to both of these arrays, when the program is done downloading, the stack window fills up with @DummyFn3 and then one @DummyFn1.
Now, if I just write to JUST one (I comment out the line for the other), it does not matter which one, the program executes as intended.
I have done some trial and error and it seems that any attempt to write to the two arrays makes the program crap out, so I am fairly certain it has something to do with the arrays.
I am totally confused. Does anyone have any idea what I should do or where I should look?
Thanks,
Charlie
解決済! 解決策の投稿を見る。