Dear All,
USBDM has been updated to V4.10.6
Please post any queries on this version in a separate thread - I really can't cope with this newfangled setup!
Documentation available at: SourceForge
Applications available at: SourceForge
Source code is available at: GitHub eventually.
bye
Note
V4.10.6 (August 2013) - This mainly concentrates on Eclipse support
Hi pgo,
I need some urgent help. Please tell USBDM is referred as stand-alone programmer. Can it be configured to program stand-alone in such a way that we press a push-button from outside and the programmer saves the target hex file and it keep programming the target controller on press of push button ? Is USBDM built to do this ? I have a USBDM JS16 based programmer. My supervisor wants update on this task, he believes USBDM can be used to program micro controllers in batch without needing a PC just like Cyclone programmer. I am stuck as i never used freescale ever. I am editting the USBDM Kinetis firmware code but it keeps giving errors.
Please respond soon with details so I can show them to my supervisor.
Hi Shayan,
Sorry USBDM does not operate in that fashion. It requires a PC to do the programming.
The stand-alone programmers refers to the software programmers that do not need a IDE such as Codewarrior to do programming.
I'm sorry if this was misleading.
bye
Dear pgo,
do you know where i can get the latest board of this design?
USBDM: USBDM/CF (combined RS08/HCS08/HCS12/Coldfire V1,2,3,4/DSC/Kinetis code) for JM32/60
I am sorry if i am posting in the wrong thread but i am looking to buy this debugger but i cant find it anywhere. I dont want to buy a chinese clone.
You can send me a pm if you want.
Thank you for your time.
Padelis
Hi Padelis,
There are a couple of suppliers on ebay doing the previous version.
I believe this link has a re-build of the current version but I'm not completely sure:
http://www.flashgenie.net/USBDM-Kinetis.html
bye
Hi zhu,
The support for MC56F devices is very limited in the programmer and the not supported in Codewarriorm10 at all.
I believe it should work with the MC56F8322. Does the stand-alone programmer work correctly?
bye
Hi PGO,
I have already made a OSBDM ,the hardware version is "USBDM_SWD_SER_JS16CWJ" and the software version is "USBDM 4.10.5",
It works very stable thanks a lot.
I have downloaded the sources version is "USBDM_JMxx_4_10_5" but is default debug configuration is"USBDM_JMxxCLD",
I change it to "USBDM_SWD_SER_JS16CWJ" but it does not work correctly.
can you give me a sources project configuration is "USBDM_SWD_SER_JS16CWJ" and can work. My mailbox is "artczq@163.com"(if
useful).
Best wishes to you.
Hi 召强 陈,
There is no separate configuration for each target. The files on GitHUB are a codewarrior project. If imported in Codewarrior then there should be multiple targets available - one for each variant.
The only configuration is done in Configure.h. This is controlled by a project level definition of the TARGET_HARDWARE. You can try manually defining such a definition:
TARGET_HARDWARE==H_USBDM_SWD_SER_JS16CWJ
bye
Dear Pgo:
Thanks for the work on 4.10.6!
I have tried the version of 4.10.6, there is something not as good as 4.10.5.
When I try to program the K20DN512 with 4.10.5 and USBDM/SWD, everything work very well,
but when I change to 4.10.6, sometimes the program flash work, sometime it not.
The following is the error figure:
It seems that one time is work and the next time is not, but the third time is work again.
Many thanks
Tao Xue
I just wanted to say a HUGE thank you for the 64-bit DEB package! It's AWESOME. The number of Linux computers running 32-bit is in the minority these days, so trying to recompile the project myself (because I run 64-bit) when I didn't know what I was doing was less than successful. The package just worked, good job!
Hi pgo,
I´d like to warn you that the 4.10.6 do not work on winXP I tried more than 3 PCs and it really don´t work. I have problems to install the driver on win 7 similar as: https://community.freescale.com/message/348546#348546
I have one PC that the 4.10.6a are working but the command line (prompt command) are not working. The command line behavior are the same as 4.10.5 but the target are not programmed.
then
I recommend use only 4.10.5b that works perfectly.
Regards.
Hi pgo. I've been having a little problem, but I didn't cared as it wasn't that bad. Now it was very important to get it fixed and I found the source of the problem.
I'm working with QG8 and I've built a very small cooperative RTOS focused on power consumption optimization, because it's going to be used on a battery powered device, so it saves a few miliamps by going into WAIT mode when it detects all tasks are idle. In the actual development stage it spends about 80% of the time in WAIT mode and uses about 30% less power.
The problem is that when accessing the variables when the processor is in WAIT, they all read zero most of the time and occasionally the right value. Tested in Variables View and also Freemaster, so it's not from CW. The workaround was just to never go to WAIT mode and everything works perfect.
As far as I remember this bug wasn't present somer versions ago, but I could be wrong.
Hope you could tell me if this is in fact a bug or it's not possible to retrieve variables in WAIT mode.
Regards.
Hi Zhilun,
I have finally got a PA4 chip to try. Unfortunately the problem is that the flash algorithm which is written in C is too large for that chip i.e. there isn't enough RAM (only 512 bytes). It will have to wait until I re-write the code in assembly for it to be practical. I'm unsure when I will have the time to look at this .
bye
Hi Zhilum,
I suggest you uninstall 4.10.6a and install 4.10.5b (USBDM_4_10_5b_Win.msi and USBDM_Drivers_1_1_0_WinXP_x32.msi)
and insert this:
You can try adding PA4 to the hcs08_devices.xml file
<device family="HCS08Plus" name="MC9S08PA4">
<clock registerAddress="0x3038" type="S08ICSV4" />
<memory type="ram">
<memoryRange start="0x0040" end="0x023F" />
</memory>
<memory registerAddress="0x3020" type="eeprom" sectorSize="2" alignment="1">
<memoryRange start="0x003100" end="0x00317F" />
</memory>
<memory registerAddress="0x3020" type="flash" securityAddress="0xFF70" sectorSize="512" alignment="4">
<securityEntryRef ref="HCS08-default-security" />
<memoryRange start="0x00F000" end="0x00FFFF" />
</memory>
<soptAddress value="0x3030" />
<sdidAddress value="0x3002" />
<sdidMask value="0x00FFFF" />
<sdid value="0x0043" />
<flashScripts>
<tclScriptRef ref="HCS08-PTxx-flash-scripts" />
</flashScripts>
<flashProgramRef ref="HCS08-PTxx-flash-program" />
</device>