Hi, I want to use FRDM-KL25Z like a debbuger using CW 10.6 so I installed USBDM_4_10_6_220_Win.msi and USBDM Drivers 1.2.0 but I get always "unknow device" instead no problem if I install USBDM 4.10.6.130 but in this case only Cw 10,5 could be used.
I'm getting crazy.
Any idea?
Thank you.
Stefano.
Solved! Go to Solution.
Hi Stephano,
Could you install using the latest drivers available here (1.3.0):
Install USBDM (version 4.6.10.230 should be available shortly) :
USBDM - Browse /Version 4.10.6/Software at SourceForge.net
Update the firmware on the board to the version available in the BDM Flash Images. See:
USBDM: Setting Up the FRDM-KL25Z
Plugin in the BDM and then check in the device manager to see what it says about the device.
bye
Hi Stephano,
Could you install using the latest drivers available here (1.3.0):
Install USBDM (version 4.6.10.230 should be available shortly) :
USBDM - Browse /Version 4.10.6/Software at SourceForge.net
Update the firmware on the board to the version available in the BDM Flash Images. See:
USBDM: Setting Up the FRDM-KL25Z
Plugin in the BDM and then check in the device manager to see what it says about the device.
bye
GREAT GREAT GRAT......IT WORKS
I love you, pgo.:smileyhappy::smileylaugh: