TBDML on Coldfire V1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TBDML on Coldfire V1

440 Views
ve3id
Contributor III

Hi,

I have been using the tbdml for a long time in the 9S12 with great success.  The other day I came across an old M5213Badge board that I would like to get some code into and use.

The tbdml is supposed to support coldfire V1, but this badge board has a 26-pint connector, which I suppose is Jtag.  The tbdml pod has a standard 6-pin bdm connector.  Are there pins on this connector that will connect to the bdm module inside the coldfire?  Sorry if this is a dumb question but I am not familiar with jtag.

Nigel Johnson

0 Kudos
1 Reply

286 Views
JimDon
Senior Contributor III

Well your basic problem is MCF5213 is a V2, not a V1, therefore it has a 26 pin BDM connector and is not supported by TBDML.