Can TBDML be used with MC9s12G48?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can TBDML be used with MC9s12G48?

ソリューションへジャンプ
562件の閲覧回数
jinhyjinhy
Contributor I

IMG_20150604_165728.gif

I got my service package for MC9S12G but however there's no connction option for TBDML?

0 件の賞賛
1 解決策
420件の閲覧回数
pgo
Senior Contributor V

Hi Jinhy,

Codewarrior not longer supports using TBDML with newer targets. It has been replace by the JM60-based OSBDM (Open Source BDM).

You can follow the procedure given at the bottom of the following page to manually add the missing information:

USBDM: Troubleshooting USBDM

If you are using USBDM (rather that the original TBDML) software then it will be necessary to re-install USBDM to have it do the updates automatically.

bye

pastedImage_0.png

The above is after installation of USBDM.

元の投稿で解決策を見る

0 件の賞賛
1 返信
421件の閲覧回数
pgo
Senior Contributor V

Hi Jinhy,

Codewarrior not longer supports using TBDML with newer targets. It has been replace by the JM60-based OSBDM (Open Source BDM).

You can follow the procedure given at the bottom of the following page to manually add the missing information:

USBDM: Troubleshooting USBDM

If you are using USBDM (rather that the original TBDML) software then it will be necessary to re-install USBDM to have it do the updates automatically.

bye

pastedImage_0.png

The above is after installation of USBDM.

0 件の賞賛