Can TBDML be used with MC9s12G48?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can TBDML be used with MC9s12G48?

Jump to solution
570 Views
jinhyjinhy
Contributor I

IMG_20150604_165728.gif

I got my service package for MC9S12G but however there's no connction option for TBDML?

0 Kudos
1 Solution
428 Views
pgo
Senior Contributor V

Hi Jinhy,

Codewarrior not longer supports using TBDML with newer targets. It has been replace by the JM60-based OSBDM (Open Source BDM).

You can follow the procedure given at the bottom of the following page to manually add the missing information:

USBDM: Troubleshooting USBDM

If you are using USBDM (rather that the original TBDML) software then it will be necessary to re-install USBDM to have it do the updates automatically.

bye

pastedImage_0.png

The above is after installation of USBDM.

View solution in original post

0 Kudos
1 Reply
429 Views
pgo
Senior Contributor V

Hi Jinhy,

Codewarrior not longer supports using TBDML with newer targets. It has been replace by the JM60-based OSBDM (Open Source BDM).

You can follow the procedure given at the bottom of the following page to manually add the missing information:

USBDM: Troubleshooting USBDM

If you are using USBDM (rather that the original TBDML) software then it will be necessary to re-install USBDM to have it do the updates automatically.

bye

pastedImage_0.png

The above is after installation of USBDM.

0 Kudos