BDM driver can't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BDM driver can't work

1,505件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

My USBDM information is as follow.

hardware:USBDM_SWD_SER_JS16CWJ_V2.0

firmware:USBDM_SWD_SER_JS16CWJ_V4

USBDM version:USBDM4.10.5

I use the BDM in win7-32bit.

First , I install the driver USBDM_Drivers_1_1_0_Win_x32.

Second I install the USBDM4.10.5.
But when I open HCS08programmer,someting wrong happened.

1, BDM can't be found

2,BDM firmware ver is 57.0.0

pastedImage_0.png

so,how can i resolve the question?

タグ(2)
0 件の賞賛
7 返答(返信)

648件の閲覧回数
pgo
Senior Contributor V

Hi Wang,

At a guess I would say that the firmware in the BDM doesn't match the version of USBDM you are using.  There was a change in the numbering that can result in the strange result you see.

Try updating the firmware with the program provided with the version you are using.

bye

0 件の賞賛

648件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

I don't update bdm firmware and just install the old driver pastedImage_0.png.

my usbdm works well.

pastedImage_1.png

but your new driver don't make it to work.

I think the driver USBDM_Drivers_1_1_0_Win_x32 result in the result.and it can't work in win7.

0 件の賞賛

648件の閲覧回数
pgo
Senior Contributor V

Hi Wang,

I am aware of some driver issues with XP which is the reason there is a separate installer for XP.  I don't know of any issues with the Windows 7 (either 32 or 64-bit).

I would appreciate if you could check if you have the same problem with the drivers just uploaded to SourceForge:

USBDM - Browse /Version 4.10.6/Software at SourceForge.net

bye

0 件の賞賛

648件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

The new driver also can't work.The result is same as USBDM_Drivers_1_1_0_Win_x32

I open my device manager,and find some information as follow:

pastedImage_0.png

is it right?



0 件の賞賛

648件の閲覧回数
pgo
Senior Contributor V

Hi Wang,

I just did a fresh install on a machine with windows 7-32bit and then installed USBDM using:

USBDM_Drivers_1_2_0_Win_x32.msi

USBDM_4_10_6a_Win.msi

and it worked without any problems so its a bit hard to suggest anything.

I also tried the USBDM_Drivers_1_2_0_WinXP_x32.msi driver which also worked.

USBDM Drivers_1_2_0_Win7_32bit.png

USBDM_Drivers_1_2_0_Win_x32.msi

USBDM Drivers_1_2_0_XP_32bit.png

USBDM_Drivers_1_2_0_WinXP_x32.msi

Could you  right-click on the device and open the Driver Details on the Driver page?

Thanks

0 件の賞賛

648件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

it cause my BDM can't work that the bdm driver setup failed in my computer.

pastedImage_0.png

what should i do to install the driver?

0 件の賞賛

648件の閲覧回数
wangbaode
Contributor IV

Hi pgo,

I right-clicked device and a dialog comes out.

pastedImage_0.png

it means that the device don't need driver files and don't load driver files.

I confirm that I installed the dirver.

0 件の賞賛