I had some trouble getting this example to run -
Solved! Go to Solution.
Hi aroy,
First, about the download process:
As explained in the video here (starting at ~ 0'40''), if you check one of the corresponding checkboxes (either for 64 or 32bit) and then click on "Download Selected Files", you should be downloading a .mltbx file. There is an issue if you just click on the file name, it starts downloading a .zip instead. The file should be the same, just the extension being altered. If you are having trouble with the download, you should consider using Internet explorer to do it. That is the recommended browser.
Second, about the licensing issue you're having, I can't reproduce it locally - can you try again, following the steps explained here (starting at ~1'45'') - you should execute this steps:
1) Go to License Keys first
2) Check the checkbox highlighted and click on Generate button.
3) Open cmd and run the vol command; it should output something like this
Volume in drive C is Primary
Volume Serial Number is D8D9-8EB6
Get the serial number and enter it (as highlighted in the image below); enter a name and then click on Generate button.
4) Save the license by either clicking on Save All, either by coping all the text below and create a license.dat file in the license folder.
Please let me know if you're still having trouble with this (and if so, please specify what MATLAB version you are using - so I can have a better chance of reproducing your exact error).
Kind regards,
Razvan.
Hi aroy,
First, about the download process:
As explained in the video here (starting at ~ 0'40''), if you check one of the corresponding checkboxes (either for 64 or 32bit) and then click on "Download Selected Files", you should be downloading a .mltbx file. There is an issue if you just click on the file name, it starts downloading a .zip instead. The file should be the same, just the extension being altered. If you are having trouble with the download, you should consider using Internet explorer to do it. That is the recommended browser.
Second, about the licensing issue you're having, I can't reproduce it locally - can you try again, following the steps explained here (starting at ~1'45'') - you should execute this steps:
1) Go to License Keys first
2) Check the checkbox highlighted and click on Generate button.
3) Open cmd and run the vol command; it should output something like this
Volume in drive C is Primary
Volume Serial Number is D8D9-8EB6
Get the serial number and enter it (as highlighted in the image below); enter a name and then click on Generate button.
4) Save the license by either clicking on Save All, either by coping all the text below and create a license.dat file in the license folder.
Please let me know if you're still having trouble with this (and if so, please specify what MATLAB version you are using - so I can have a better chance of reproducing your exact error).
Kind regards,
Razvan.
Thanks Razvan! That sorted it out.
Do you have any input on #3?
Arunesh
Hi aruneshroy
In respect with:
- On rolling back to the EAR 0.4, I tried running the code listed above but found the functions ‘rangeFFT’, ‘dopplerFFT’ and ‘peaksearch3D’ missing. Are they listed somewhere?
The functions rangeFFT, dopplerFFT and peaksearch3D are part of the Radar SDK package.
These can be found into: ..\{RADAR SDK INSTALL PATH}\Tools\SPT_bitexact_model\src
To use them, simply download the RSDK package and add that folder to the MATLAB Path.
The Radar SDK are available for download in your Software Account.
Hope this helps!
Daniel