Smart Pump Monitor Demo
This demo shows a small water pump rig consisting of a water pump and 3 valves put together to collect data for supervised machine learning. Normal operation as well as abnormal conditions may be simulated with the rig. There are 2 sensor boards attached by clamps to the water pipe. Each sensor board has many sensors on it, but only the accelerometer will be used to gather the data. One board is used for data logging. The other runs a model which was generated via machine learning based on data logged from the first board. Pump vibration measurements are processed through the model by the MCU on that board to determine the operating state of the system
Features
Links
Related demos
We are providing the Best Data Science Course Training Institute in Pune with Job assistance & offers a blended model of data science training. It helps you to master in Python, ML, Git, etc. to become a certified Data Scientist. Enroll in the best training now!