i'm looking at using the NT3H2111 for nfc at 13.56MHz. Can you recommend an off-the-shelf reader that has a USB interface to a PC, as well as PC software, that would work with this nxp part? also, i need the usb reader to be able to read and write to the NT3H2111 memory
thanks,
Stu
Dear stuart dejonge,
Hope you are doing great, the reader that comes to my mind is the PEGODA Contactless Smart Card Reader based on MFRC523|NXP , it communicates to your PC using USB also has its own software RFIDDiscover|NXP , there are two versions of the software the public one and the NDA version which comes with more features this reader can write to NTAG i2C, please check this if you want to sign NDA please submit an internal ticket Support|NXP.
Have a great day !