你好,请问lcrc663能否支持wiegand协议?我看数据手册只有
• ISO/IEC14443A/MIFARE
• ISO/IEC14443B
• FeliCa
• ISO/IEC15693/ICODE
• ICODE EPC UID
• ISO/IEC 18000-3 mode 3/ EPC Class-1 HF 这几种,并没有看到支持wiegand协议,谢谢
wiegand协议和ISO 14443A这些协议不是一个概念吧,wiegand一般是指数据存储的格式,https://www.nxp.com/docs/en/application-note/AN10957.pdf?fsrch=1&sr=2&pageNum=1
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------