hi,
we can get calibration data from Cockpit. And Cockpit has a button to update EEPROM with new DPC calibration result..
I want to update EEPROM of another board with the same values.
I checked "secure f/w update library", where I could see OPCODEs for accessing EEPROM.
Similary, I guess there will be for DPC area.
/* OPCODES */
#define PH_DLHAL_HW_PN5180_DL_OPCODE_DL_RESET 0xF0 /**<This command resets the IC. */
#define PH_DLHAL_HW_PN5180_DL_OPCODE_DL_GETVERSION 0xF1 /**<This command provides the firmware version. */
#define PH_DLHAL_HW_PN5180_DL_OPCODE_DL_GETDIEID 0xF4 /**<The command returns the die ID. */
BTW. I looks that Reader Library doesn't have EEPROM update feature. How can I update EEPROM?
BR,
Devin
解決済! 解決策の投稿を見る。
Hi Devin,
the NFC Cockpit allows a <dump EEPROM> (=store EEPROM into a file) + <load EEPROM> (store the file Content into the EEPROM).
For the same functionality in an own code, the PN5180 commands must be used.
For the "normal" area, containing the general settings and LUTs:
WRITE_EEPROM
READ_EEPROM
For the "Load Protocol" area:
UPDATE_RF_CONFIG
RETRIEVE_RF_CONFIG
BR,
Jimmy
Hi Devin,
the NFC Cockpit allows a <dump EEPROM> (=store EEPROM into a file) + <load EEPROM> (store the file Content into the EEPROM).
For the same functionality in an own code, the PN5180 commands must be used.
For the "normal" area, containing the general settings and LUTs:
WRITE_EEPROM
READ_EEPROM
For the "Load Protocol" area:
UPDATE_RF_CONFIG
RETRIEVE_RF_CONFIG
BR,
Jimmy