What does this result mean on TagInfo?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What does this result mean on TagInfo?

2,056 Views
simonsimonli
Contributor I

I was unable to retrieve the required information requested by the client off provided badges. I used Taginfo to retrieve the following images. Are the cards programmed correctly? Are there information that can be read of the cards? Any help is appreciated. Thanks. 

Labels (1)
0 Kudos
3 Replies

2,028 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

You may check it via the threads as the links

URL:https://community.nxp.com/t5/Other-NXP-Products/Mifare-classic/td-p/1236389.

https://community.nxp.com/t5/NFC/NXP-Taginfo-app-just-doesn-t-read-tags-on-iphone/m-p/839907

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos

2,023 Views
simonsimonli
Contributor I

Thanks for the reply, but I'm not sure I understand you. 

I was provided with these badges. They are supposed to be programmed with the correct numbers/data

I was also provided with the AID, KEY etc. to program the reader with. But so far I got no response from the readers I used. 

So I scanned them with TagInfo on my phone and got the above results.

Just wondering if anyone can tell me if these cards were programmed correctly by the providers?

0 Kudos

2,017 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

From the above Pictures there is no problem. The program of this card can't be read by TagInfo, if the program is encrypted. Please find the Taginfo's feature as the link.

URL:https://play.google.com/store/apps/details?id=com.nxp.taginfolite.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos