Hi Steve,
Could you tell us which MCU are you using?
Thanks in advance!
Best Regards,
Carlos Mendoza
Technical Support Engineer
Hello Steve,
-Can LPCXpresso detect the LPC-Link2 when debugging?
-How are the jumpers on LPC-Link2 being shorted?
-Can you build the project you are working with successfully?
Could you please provide us with additional information on this request?
Regards,
Ivan.
Ivan,
After re-configuring Windows>Prefs>LPCXpresso to use the right MCU and LPC-Link2, and after running Boot Debug Probe, I attempted to reprogram the flash, but got this message:
In my Windows devs & printers panel, the LPC device name changed to "LPC-LINK2 CMSIS-DAP V5.147". Encouraging?
Like I said, I'm a noob with this API & its debug.
Hi Ivan,
FlashMagic can detect and work through the LPC-Link2 fine. I cannot tell whether LPCXpresso is detecting it or not.
The jumpers are set normally: JP1 is open, JP2 is shorted.
The project builds successfully both in Release and Debug mode.
I have two info’s in the problems report that might point to something:
Description Resource Path Location Type
Bad function name "defaultIntHandler" (pattern /^[A-Z_]/) startup.c /lib_chip_nss/mods/startup line 60 Code Analysis Problem
Bad function name "defaultResetISR" (pattern /^[A-Z_]/) startup.c /lib_chip_nss/mods/startup line 70 Code Analysis Problem
Debug just fails to run.
Steve