How to reconfigure the NHS3100 startup state to take temperature measurements only under NFC field in battery-less application?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to reconfigure the NHS3100 startup state to take temperature measurements only under NFC field in battery-less application?

ソリューションへジャンプ
2,477件の閲覧回数
stevewald
Contributor III

We need to reconfigure the NHS3100 startup state to take temperature measurements only under NFC field for a battery-less application. I don't see where in the TLogger sources that the initial state is configured. Can someone provide some hints or clues?

1 解決策
2,224件の閲覧回数
driesmoors
NXP Employee
NXP Employee

The current firmware (SDK 10.1) will already make a temperature measurement each time is tapped by the phone, regardless whether it is configured or not. This value is also passed along in the NFC shared memory as a text record. You can have a look at that when you use the phone without any APP being active.

Have a look at

  • Init, file maintlogger.c, where TMeas_Measure is called.
  • ResponseCb, file msghandler.c, where NDEFT2T_CreateTextRecord is called.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,225件の閲覧回数
driesmoors
NXP Employee
NXP Employee

The current firmware (SDK 10.1) will already make a temperature measurement each time is tapped by the phone, regardless whether it is configured or not. This value is also passed along in the NFC shared memory as a text record. You can have a look at that when you use the phone without any APP being active.

Have a look at

  • Init, file maintlogger.c, where TMeas_Measure is called.
  • ResponseCb, file msghandler.c, where NDEFT2T_CreateTextRecord is called.
0 件の賞賛
返信
2,224件の閲覧回数
stevewald
Contributor III

Dries Moors had earned a badge for giving us more than this answer, including some source code to run a cleaner no-battery use case on the NHS3100. There are subtle problems with the initialization without a battery to maintain state. Thanks!

2,224件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

It is only required to flash the NHS3100 with TLogger example. You will be able to take temperature measurements every time you approach your phone to the device. This is accomplished because of the phone's field power provided to the device even if NHS3100 is no longer battery powered.

 

Regards,

Ivan.

0 件の賞賛
返信