TagXplorer v1.2 by NXP Software identifies all tags as NTAG 203X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TagXplorer v1.2 by NXP Software identifies all tags as NTAG 203X

1,566 Views
vince1
Contributor II

#Hello community,

 

I have a problem using TagXplorer v1.2 by NXP Software connected to the NXP Pegoda CLRD710 Reader, running on my Windows 10 PC.

 

TagXplorer Version: 1.2

Build Version: 2019-12-14 175055

TapLinx SDK Version: 1.5

NXP Pegoda CLRD710 Firmware 2.2.8

 

Regardless of the Tag Type I place on the Pegoda Reader, when TagXplorer connects to the tag, the tag is identified as an NTAG 203X (I am using an NTAG 213 Tag Tamper).  Then I am not able to execute any of the NTAG Operations appropriate for the NXP tag type I have.  I get a “Tag is not of type…” Error.

 

Can anyone suggest how I can configure TagXplorer to connect to the tag with the correct tag type?

 

Thanks,

Vince

Labels (2)
1 Reply

1,483 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

The topic has already been addressed in the following thread: https://community.nxp.com/thread/518272 

The bug was already reported to the development team and will be corrected on the next release.

Thank you for your feedback.

BR,

Ivan.