TagXplorer - ACR 1281U-C1 not listed in readers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TagXplorer - ACR 1281U-C1 not listed in readers

ソリューションへジャンプ
2,354件の閲覧回数
softzer0
Contributor II

I have the reader in the subject and I'm using Windows 10 with correctly installed drivers for it, as it can be seen in the attachment. When I open TagXplorer application, it says that no reader is connected. Can anyone tell me what should I do?

softzer0_0-1600257378443.png

 

0 件の賞賛
返信
1 解決策
2,344件の閲覧回数
softzer0
Contributor II

This is solved somehow by restarting the computer after installing drivers. This topic can be closed.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,345件の閲覧回数
softzer0
Contributor II

This is solved somehow by restarting the computer after installing drivers. This topic can be closed.

0 件の賞賛
返信
2,337件の閲覧回数
acesinvensys
Contributor I

If possible please share drivers 

0 件の賞賛
返信
2,335件の閲覧回数
softzer0
Contributor II

I have downloaded these and installed them manually: https://www.acs.com.hk/download-driver-unified/10903/ACS-Unified-Driver-Win-4300.zip

0 件の賞賛
返信
2,339件の閲覧回数
acesinvensys
Contributor I

Are you able to read tags using this reader. 

 

0 件の賞賛
返信
2,332件の閲覧回数
softzer0
Contributor II

Yes, I’m able to do everything.

0 件の賞賛
返信