SN110 failed to detect card by pnscr

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SN110 failed to detect card by pnscr

跳至解决方案
2,021 次查看
feifeihu
Contributor II

SEND : 4 > 20000100
RCEIVE : 4 < 40000100
RCEIVE : 13 < 60000A02002004050FA4011034
SEND : 5 > 2001020000
RCEIVE : 33 < 40011E001A3E0600010604FFFF01FF000800000100020003008000820083008400
SEND : 6 > 20030301A044
RCEIVE : 9 < 4003060001A0440100
SEND : 4 > 20000100
RCEIVE : 4 < 40000100
RCEIVE : 13 < 60000A02002004050FA4011034
SEND : 5 > 2001020000
RCEIVE : 33 < 40011E001A3E0600010604FFFF01FF000800000100020003008000820083008400
SEND : 3 > 2F0200
RCEIVE : 8 < 4F02050000014579
SEND : 6 > 20030301A007
RCEIVE : 9 < 4003060001A0070100
SEND : 6 > 20030301A08E
RCEIVE : 9 < 4003060001A08E0101
SEND : 8 > 20020501A08E0101
RCEIVE : 5 < 4002020000
SEND : 6 > 20030301A00F
RCEIVE : 40 < 4003250001A00F200000000000000000000000000000000000000000000000000000000000000000
SEND : 6 > 20030301A00F
RCEIVE : 40 < 4003250001A00F200000000000000000000000000000000000000000000000000000000000000000
SEND : 8 > 20020501A0440100
RCEIVE : 5 < 4002020000
SEND : 51 > 20023001A00E2CF0003E11E4E4E40000000000A78EFFFF0F0F0F0F0A0000000002000001001000040000001740200713070513
RCEIVE : 5 < 4002020000
SEND : 8 > 20020501A0D40101
RCEIVE : 5 < 4002020000
SEND : 6 > 20030301A10B
RCEIVE : 9 < 4003060001A10B0100
SEND : 6 > 20030301A015
RCEIVE : 9 < 4003060001A0150101
SEND : 6 > 20030301A095
RCEIVE : 9 < 4003060001A0950100
SEND : 61 > 20023A04A0EC0101A0ED0101A0682A0640600319000000008204000002000F0002000FA000A00003FA0000004C0014007D00057F0000010003A00A0120
RCEIVE : 5 < 4002020000
SEND : 58 > 200237112801002101003001083101033201603801013304010203045401065001025B01003E010080010181010182010E180101680101850101
RCEIVE : 5 < 4002020000
SEND : 6 > 20030301A011
RCEIVE : 15 < 40030C0001A01107010A3201C8F6F6
SEND : 6 > 20030301A00F
RCEIVE : 40 < 4003250001A00F200000000000000000000000000000000000000000000000000000000000000000
SEND : 6 > 20030301A085
RCEIVE : 12 < 4003090001A085045008A82C
SEND : 9 > 20020601A01D020000
RCEIVE : 5 < 4002020000
SEND : 3 > 2F2100
RCEIVE : 4 < 4F210100
SEND : 4 > 20000100
RCEIVE : 4 < 40000100
RCEIVE : 13 < 60000A02002004050FA4011034
SEND : 5 > 2001020000
RCEIVE : 33 < 40011E001A3E0600010604FFFF01FF000800000100020003008000820083008400
SEND : 6 > 20030301A00F
RCEIVE : 40 < 4003250001A00F200000000000000000000000000000000000000000000000000000000000000000
SEND : 5 > 2003020100
RCEIVE : 9 < 40030600010002E803
SEND : 5 > 2003020129
RCEIVE : 7 < 40030400012900
SEND : 5 > 2003020161
RCEIVE : 7 < 40030400016100
SEND : 5 > 2003020160
RCEIVE : 8 < 4003050001600108
SEND : 16 > 21000D04040302050303030201800180
RCEIVE : 4 < 41000100
SEND : 3 > 220000
RCEIVE : 5 < 4200020003
RCEIVE : 11 < 6200088001000103010200
RCEIVE : 11 < 6200088101000103018100
RCEIVE : 11 < 620008C00100010301C001
SEND : 5 > 2201021001
RCEIVE : 4 < 42010103
SEND : 6 > 010003810201
RCEIVE : 6 < 600603010101
CORE_CREDIT_NTF OK !!!
RCEIVE : 5 < 0100028186
SEND : 11 > 01000881010302808182C0
RCEIVE : 6 < 600603010101
CORE_CREDIT_NTF OK !!!
RCEIVE : 5 < 0100028186
SEND : 5 > 2201028001
RCEIVE : 4 < 42010100
RCEIVE : 4 < 62010103
SEND : 6 > 010003810204
RCEIVE : 6 < 600603010101
CORE_CREDIT_NTF OK !!!
RCEIVE : 5 < 0100028186
SEND : 5 > 2201028101
RCEIVE : 4 < 42010100
RCEIVE : 4 < 62010103
SEND : 6 > 010003810204
RCEIVE : 6 < 600603010101
CORE_CREDIT_NTF OK !!!
RCEIVE : 5 < 0100028186
SEND : 5 > 220102C001
RCEIVE : 4 < 42010100
RCEIVE : 9 < 610A06010003C08004
RCEIVE : 4 < 62010100
RCEIVE : 9 < 610A06010003C08104
SEND : 6 > 010003810204
RCEIVE : 9 < 610A06010003C08203
RCEIVE : 6 < 600603010101
CORE_CREDIT_NTF OK !!!
RCEIVE : 5 < 0100028186
SEND : 5 > 220302C001
RCEIVE : 4 < 42030100
SEND : 5 > 2003020152
RCEIVE : 8 < 4003050001520104
SEND : 7 > 20020401850101
RCEIVE : 5 < 4002020000
SEND : 3 > 2F2100
RCEIVE : 4 < 4F210100
SEND : 4 > 20090100
RCEIVE : 4 < 40090100
SEND : 7 > 20020401020101
RCEIVE : 5 < 4002020000
SEND : 26 > 20021701291446666D010112020207FF03020003040164070103
RCEIVE : 5 < 4002020000
SEND : 19 > 20021005300104310100320120380101500100
RCEIVE : 5 < 4002020000
SEND : 8 > 200205010002F401
RCEIVE : 5 < 4002020000
SEND : 20 > 2103110800010101020103018001810182010601
RCEIVE : 4 < 41030100
PRESENT READER OR CARD !!!
SEND : 4 > 21060100
RCEIVE : 4 < 41060100
SEND : 45 > 21012A00070209103BD27600008501011202C0390103C03B0401030001050003C03B000003C03B010003C03B02
RCEIVE : 4 < 41010100
SEND : 20 > 2103110800010101020103018001810182010601
RCEIVE : 4 < 41030100
PRESENT READER OR CARD !!!
RCEIVE : 4 < 600701A1
Card Detected !!!

 

could you please help parse?Especially the meaning of the notification of "600701A1".

Thanks!

0 项奖励
回复
1 解答
1,983 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @feifeihu ,

 

SN110 is not a MM product and just supported by Disty only, please contact your local Disty for the right tool to analyze this issue.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,006 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @feifeihu ,

 

I am sorry, but this part is not supported by this channel, please kindly contact your local Disty or NXP sales representatives for further help on this.

 

Thanks for your patience and understanding!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,002 次查看
feifeihu
Contributor II

as you have done similar analyze before here:

https://community.nxp.com/t5/NFC/PN7120-StartDiscovery-returns-DISCOVERY-ALREADY-STARTED/m-p/672335

 

Please provide same thing or some tools to let me analyze the data.

0 项奖励
回复
1,984 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @feifeihu ,

 

SN110 is not a MM product and just supported by Disty only, please contact your local Disty for the right tool to analyze this issue.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复