PN7462 NFC Read card number problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 NFC Read card number problem

3,046 Views
steven123456
Contributor I

Hi, I use PN7462AUHN design a board and use UART interface.

The internal regulator (DVDD, PVDD_OUT) work normally. TVDD_IN(PIN34) use 5V external supply.

Antenna side (TX1 TX2) we according to NXP antenna design guide to matching. Output power is 14dbm but finally can't read card number. Firmware on PN7462 EVB can read card successfully.

I want to ask maybe what kind of problem will cause fail to read card number?

Attached is my antenna test result and VNA measured result. 

 

0 Kudos
Reply
3 Replies

3,026 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello Steven,

 

Thanks for the information! Looks like it is an antenna tuning issue, from VNA.png, the point 1 is a little bit far from the straight line across the smith chart, you should tune it right on this line, something like Fig 33 in AN11706. Please kindly refer to https://www.nxp.com/docs/en/application-note/AN11706.pdf for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,019 Views
steven123456
Contributor I

Hi Kan,

Thanks for your reply. And I want to ask other question about matching.

1.When i use VNA measure tx1 and tx2 impedance, should I soldering the main chip and other components (about Rx and ANT components) on the broad?

Or use empty PCB board just soldering TX1, TX2 matching components?

2. I read NXP document AN11755, in this document mention symmetrical and asymmetrical tuning, should PN7462 use symmetrical tuning in AN11755? Or must same as AN11706 tuning method?

Best regards.

@Kan_Li 

0 Kudos
Reply

2,987 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @steven123456 ,

 

1.When i use VNA measure tx1 and tx2 impedance, should I soldering the main chip and other components (about Rx and ANT components) on the broad?

Or use empty PCB board just soldering TX1, TX2 matching components?

 

- It is ok to leave the main chip and other components (about Rx and ANT components) on the broad when you use VNA measure tx1 and tx2 impedance. just note no power supply during the measurement.

2. I read NXP document AN11755, in this document mention symmetrical and asymmetrical tuning, should PN7462 use symmetrical tuning in AN11755? Or must same as AN11706 tuning method?

- Normally both methods can be applied for PN7462, but if you enable DPC, symmetrical tuning is recommended, please kindly refer to section 2.2 in https://www.nxp.com/docs/en/application-note/AN11741.pdf for more details. and yes, please use  AN11706 for antenna design based on PN7462.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply