Not getting sine wave when TX-LDO is operating at 3V(external tvdd)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not getting sine wave when TX-LDO is operating at 3V(external tvdd)

943 Views
gokulkrishna
Contributor I

We are observing no change in wave-forms when the TXLDO_CONTROL_REG is changed. The TXLDO is configured as follows:

PH_REG_CLEAR_BIT(PMU_TXLDO_CONTROL_REG, TXLDO_ENABLE);
PH_REG_CLEAR_BIT(PMU_TXLDO_CONTROL_REG, TXLDO_LOW_POWER_EN);
PH_REG_CLEAR_BIT(PMU_TXLDO_CONTROL_REG,TXLDO_ENABLE_LP2);
PH_REG_SET_BIT(PMU_TXLDO_CONTROL_REG, TXLDO_LIMITER_EN);
PH_REG_SET_BIT(PMU_TXLDO_CONTROL_REG, TXLDO_OVERCURRENT_EN);
PH_REG_SET(PMU_INTERRUPT_SET_ENABLE_REG,PMU_INTERRUPT_SET_ENABLE_REG_TXLDO_OVERCURRENT_IRQ_SET_ENABLE_MASK);
PH_REG_SET_FIELD(PMU_TXLDO_CONTROL_REG, TXLDO_SELECT,E_TVDD_3M0_V);//3volt
PH_REG_SET_BIT(PMU_TXLDO_CONTROL_REG, TXLDO_ENABLE);

PH_REG_SET_FIELD(PMU_TXLDO_CONTROL_REG, TXLDO_SELECT_ANT,0x03);// TXLDO_DET_OUT  range of 100mA

No NFC cards are able to detect with the current wave-form.

#pn7462au‌ #TXLDO #pn7462 low power#pn7462au fw & sw examples#nfc.

0 Kudos
Reply
2 Replies

775 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please let me get confirmation from internal team about your request. Will come back asap.

Regards,

Ivan.

0 Kudos
Reply

775 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please see below answer from Apps team expert:

With the Settings on the TxLDO, you will not be able to Change the wave form. the TxLdo is only to deliver the Output power that is provided to the TVDD_Out pin, the shaping and wave-forms are set in different Registers. To Change or optimize you waveform see Antenna design guide AN11706  (Section 4.4 and following).

Regards,

Ivan.