OM5578 vs OM5577 field strength

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM5578 vs OM5577 field strength

1,253 Views
jan_visser
Contributor II

OM5578 reader field strength vs OM5577.

Hi, I am developing a NFC reader solution. The tags that I am using have a very small antenna and therefore need a strong field to work properly.

I was looking at the two NFC controller SBC  kits (OM5577 and OM5578) and was wondering which one would have the strongest antenna field. I would think that would be the OM5578 since it has a higher voltage for the antenna drive circuit. Is my assumption correct?

Labels (2)
0 Kudos
Reply
2 Replies

1,141 Views
jan_visser
Contributor II

Hello Ivan,

I've bought both an OM5577 and an OM5578 and did some measurements with a sniffer probe attached to an oscilloscope. The voltage induced in my probe by the OM5578 is about 2 times that of the voltage induced by the OM5577. Also, I could read tags over a larger distance with the OM5578 than with the OM5577.

I'm familiar with the tables in the user manual that you mention. I suspect that the RF performance tables for one of these devices is copied from the other because they are exactly the same for both. 

Regards,

Jan

0 Kudos
Reply

1,141 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

In chapter 4. of PN7120's User manual, it is shown the Voltage measured with EMVCo reference PICC (Proximity Inductive Coupling Card): https://www.nxp.com/docs/en/user-guide/UM10878.pdf 

Which is the same as the PN7150's measurements described in chapter 4.2: https://www.nxp.com/docs/en/user-guide/UM10935.pdf 

Regards,

Ivan.

0 Kudos
Reply