NXP Tagwriter - Write from CSV

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Tagwriter - Write from CSV

3,623件の閲覧回数
chrisong_what
Contributor I

Hi Sir/Madam,

 

Good day to you.

 

Kindly check with you the CSV file if i want to add more records in a row, is it possible can do?

 

Thanks.

 

Best Regards, 
Christopher

タグ(3)
0 件の賞賛
返信
3 返答(返信)

3,322件の閲覧回数
t_kubicek
Contributor I

Hallo, could you please provide me the correct vcard template how to write multiple contacts eg. up to 200 contacts via NFC NXP TAGWriter into multiple NFC cards.

Please check also my template attached which NXP writer does not accept.

Thanks

Thanks Tomas

 

0 件の賞賛
返信

3,496件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Thank you for contacting us. I just checked your case; basically the app allows you to write comma separated values but not more than one record per row, this means that despite you write it either on CSV or "normal" format, you could only add one record per row, please see below for an example of the Comma Separated Value:

pastedImage_2.png

Have a nice day!

BR,

Ivan.

0 件の賞賛
返信

577件の閲覧回数
sipos93
Contributor I

Hi @IvanRuiz 

Could I also request a sample of how the CSV content should look like for the application to accept it?
I just want to save plain URL addresses.

For example:
https://1.com
https://2.com
https://3.com

0 件の賞賛
返信