Hello, recently I acquired a new NHS3100 SensorBoard for testing its functionality.
I installed the Android App SensorBoard Monitor on my cellphone, connected to the board and it seems ok, I can log the Temperature, Humidity, and sense some Tilting information.
However, this is not exactly what I expect. I would like to measure the output of the accelerometer for measuring pitch and roll angles. Is there a way that I can communicate with the board using JTAG (LPC-Link 2), read these values on Windows 10 and log the accelerometer information just like the Temperature and Humidity?
I have installed the LPCXpresso software on my computer, but do not have any clue of how to communicate with the board.
Thank you very much
已解决! 转到解答。
Hi,
In the SensorBoard Monitor demo, the FXLS accelerometer is configured to report threshold excursions, and based on that, different events are deduced. The firmware application running on the NHS3100 does not interpret the raw XYZ data. This is done on purpose to save battery life, as it allows the NHS3100 IC to spend more time in deep power down mode.
It is definitely possible to work with the raw accelerometer data, and 'live stream' them to your PC.
Some pointers:
Kind regards,
Dries.
Hi,
In the SensorBoard Monitor demo, the FXLS accelerometer is configured to report threshold excursions, and based on that, different events are deduced. The firmware application running on the NHS3100 does not interpret the raw XYZ data. This is done on purpose to save battery life, as it allows the NHS3100 IC to spend more time in deep power down mode.
It is definitely possible to work with the raw accelerometer data, and 'live stream' them to your PC.
Some pointers:
Kind regards,
Dries.