How to connect FRDM-K82F and CELV6630ARD Together?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect FRDM-K82F and CELV6630ARD Together?

1,545 Views
tom_porter
Contributor I

I purchased a FRDM-K82F dev board and the CLEV6630ARD NFC development board. NXP says they work together, so was able to download the MCUXpresso, got the sample projects. However are the boards supposed to connect directly on top of each other? If yes how do they do so? If not, do I have to manually jumper the wires between the boards to connect them?

Thanks,

Tom

Labels (1)
0 Kudos
Reply
4 Replies

1,470 Views
tom_porter
Contributor I

Hi,

Thanks but the link that you sent, I get an unauthorized message...

Can you copy that thread into this one so I can see it? 

Thanks,

Tom

0 Kudos
Reply

1,470 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I can open the thread correctly. And you can find the related information as the below:

pastedImage_1.png

Have a nice day

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply

1,470 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the more information as the thread. FRDM-K82F and CLEV6630ARD issues .

Hope it help you. Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply

932 Views
fabiotartaglion
Contributor I

I have the same problem with FRDM K82 and CLEV6630ARD.

The issues link not work for me (browser display 'i have not previlege').

Please can You provide another way to access the lssues link ?

Thank's in advance.

 

Fabio T.

0 Kudos
Reply