Hi NXP Community. I am using a MCU from the KEA family and a NFC frontend from the CLRC663 Family. Can the NFC Reader Library be used with this MCU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi NXP Community. I am using a MCU from the KEA family and a NFC frontend from the CLRC663 Family. Can the NFC Reader Library be used with this MCU?

581 次查看
joseph_kielasa
Contributor I

MCU: s9kea64p64m20sf0

NFC: CLRC66303

标签 (2)
0 项奖励
回复
1 回复

484 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Compared to an LPC1769 or a Kinetis K82, it is a very limited Hardware. If you are looking for an automotive MCU with Higher performance, it would be interesting to take a look to the S32K family:

32-bit Automotive General Purpose MCUs|NXP 

Once you find the correct MCU for the porting, it would be helpful to refer to the following document:

NFC Reader Library Porting to i.MX RT1050 

I hope this helps.

Regards,

Ivan.

0 项奖励
回复