Can this CLRC663 / SLRC610 be directly connected to PLC using RS232/RS485(With the help of MAX232/rs485 transceivers) or requires an external controller?
Hello,
CLRC663 / SLRC610 can be directly connected to PLC using RS232/RS485(With the help of MAX232/rs485 transceivers).
Hope it help you. Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------