CLRC663 NFC RS232

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 NFC RS232

647 Views
lakshminarayana
Contributor II

Can this CLRC663 / SLRC610 be directly connected to PLC using RS232/RS485(With the help of MAX232/rs485 transceivers) or requires an external controller?

0 Kudos
Reply
1 Reply

631 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

CLRC663 / SLRC610 can be directly connected to PLC using RS232/RS485(With the help of MAX232/rs485 transceivers).

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply