有没有一种方案代替PN7462在Android系统上实现NFC和PSAM的功能

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

有没有一种方案代替PN7462在Android系统上实现NFC和PSAM的功能

2,250 Views
13102370205
Contributor I

我们的CPU 是MTK6737,想在Android系统上实现NFC 和PSAM功能,本来想使用PN 7462实现功能,但是新手一枚,在没有资料的情况下没有完成,现在想寻求一种方案,实现这个功能

0 Kudos
Reply
3 Replies

1,761 Views
Kan_Li
NXP TechSupport
NXP TechSupport

请问你们做的是什么设备?POS?

0 Kudos
Reply

1,761 Views
13102370205
Contributor I

是的。我在做POS。在MTK平台上,Android版本为6.0

13102370205@163.com

发件人: Kan_Li

发送时间: 2017-05-09 11:16

收件人: 小雨 李

主题: Re: - Re: 有没有一种方案代替PN7462在Android系统上实现NFC和PSAM的功能

NXP Community

Re: 有没有一种方案代替PN7462在Android系统上实现NFC和PSAM的功能

reply from Kan_Li in NFC - View the full discussion

请问你们做的是什么设备?POS?

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in NFC by email or at NXP Community

Following Re: 有没有一种方案代替PN7462在Android系统上实现NFC和PSAM的功能 in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 Kudos
Reply

1,761 Views
Kan_Li
NXP TechSupport
NXP TechSupport

如果是Android POS一般都会另外再挂一个不跑系统或者跑实时操作系统的安全MCU再接非接和接触式模块, 你可以使用K21/K81/i.Max + RC663的方案。

 

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply