PN7160 - Extended NFC Factory Test Application for Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7160 - Extended NFC Factory Test Application for Linux

PN7160 - Extended NFC Factory Test Application for Linux

Extended NFC Factory Test Application includes: 

  • Get Current value (current measurement in mA)
  • DPC Check (Available from FW. Version 12.50.06)
  • Get AGC Value 
  • Get AGC Value NFCLD (AGC value reading with fixed NFC Level Detector level)
  • Dump EEPROM settings 
 
EEPROm_dump.png
How to get it: 
  1. Just download the app from Github.
  2. Replace the "NfcFactoryTestApp.c" with the file which is here in the attachment. 
  3. Run the application as described in ->AN13287.

 

Tomas Parizek 

Customer Application Support 

Labels (1)
Attachments
Comments

Can you provide the Android version

7160芯片,android 14 ,NFC FW 12.50.09

使用getAGC时返回值不对,请问是什么问题 

 

mark_tang_0-1718936125259.png

 

Hello mark_tang, 

 

For Android, You should just extend the code in the same way as for Linux. Then it should work. 

 

About the AGC value, yes it is strange. You are getting quite a high value, let me double-check the AGC range. 

 

Thanks ! 

 

BR

Tomas 

100% helpful (1/1)
Version history
Last update:
3 weeks ago
Updated by: