I want to develop High Voltage PMSM Motor drive application. I have bought HVP-MC3PH.
I can find 2 different PMSM examples.
So which SDK i should use?
And why motor is not running smooth with latest SDK 2.7.0?
Hi Ritesh,
Sorry for the late reply.
We always recommend to use our latest available tools. Which is the case of SDK 2.7.0. In addition, please check the SDK folder in the following path.
SDK installation folder\middleware\motor_control\pmsm
There you will find FRAC version for PMSM motor control.
I hope this helps!
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Felipe,
Thanks for the Reply.
Where can i find Change log of PMSM Motor SDK between following versions?
The Differences which i have found..
Hi Ritesh,
Unfortunately, we do not have any log with the changes between this versions. I am sorry for the inconveniences that this may cause you.
Best regards,
Felipe