Freemaster V2.0 communication lost after opening project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster V2.0 communication lost after opening project

1,479 Views
bernharddavid
Contributor I

Need Help please !

 

I am Working with KDS Version: 3.2.0 with a TWR_KV11Z75M Development Kit. I use the predefined Project pmsm_ref_sol build release code and let it run using seggerlink V512g for communication.

When  start Freemaster V2.0 I can connect via seriell Com Interface but after selection of the example project connection is lost and variables are unknown.

 

153155_153155.PNGCapture.PNG

Labels (1)
0 Kudos
1 Reply

1,077 Views
ivadorazinova
NXP Employee
NXP Employee

Hi,

This message is probably caused by an error with COM port.

Project -> Options

Please, are you sure with your communication settings?

freemaster.png

Please refer to Project Options - Communication link below:

FreeMASTER for Embedded Applications - Communication

Please let me know if you solved your issue.

Have a nice day.

Iva

0 Kudos