how to debug the motor control example by KDS with MKV31F128VLH10?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to debug the motor control example by KDS with MKV31F128VLH10?

1,678 Views
armaghanbahari
Contributor I

hello, I'm new to KDS, and I want to control an induction motor by V/F method. I use MKV31F128VLH10 and I downloaded the motor example which is available in NXP.com

But it does not work and I don not know how to modify this project in order to become suitable for this MCU.

there is no problem with build and debug.

These errors are appeared when the example project is debugging into the micro controller:

Reading all registers

Removing breakpoint @ address 0x00003688, Size = 2

Read 4 bytes @ address 0x000004E8 (Data = 0xBFFEF7FF)

WARNING: Failed to read memory @ address 0x2000FFF4

Reading 64 bytes @ address 0x2000FFC0

WARNING: Failed to read memory @ address 0x2000FFC0

Reading 64 bytes @ address 0x2000FFC0

WARNING: Failed to read memory @ address 0x2000FFC0.

Labels (1)
0 Kudos
Reply
1 Reply

1,211 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

If you are debug the 3-phase AC Induction Motor Control demo with HVP-KV31F120M board?

I had tried to debug the  <build_demos> based on KDS IDE software & HVP-KV31 board without any problem.

Thank you for the attention.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply