Profiler block with referenced models not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Profiler block with referenced models not working

736件の閲覧回数
Oliver3
Contributor I

Hello,

we are working with the NXP Toolbox and encountered a Problem with the Profiler block, when using it within referenced models: 

If building the referenced model as Top-Model, no error occurs. If building the overall model, during the referenced model build the following error occurs ('missing files'):

Function_Call_Subsystem_private.h:27:29: fatal error: s32k_clock_init.h: No such file or directory #include "s32k_clock_init.h"

Please see also the attachement (example from Profiler with an additional referenced mode).

Is there any workaround or bugfix for this? 

Thank you,

Oliver

0 件の賞賛
返信
0 返答(返信)