How to transplant the dual motor control S32 project to Codewarrior IDE5.90?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to transplant the dual motor control S32 project to Codewarrior IDE5.90?

1,561 Views
edenli
Contributor V

Hi Daniel,

Now I found the software of S32 Design Studio for Power Architecture v1.2 has some error,So i wanna transplant the dual motor control S32 project(http://www.nxp.com/downloads/en/apps/MTRCKTDPS5643L_SW.exe ) to Codewarrior IDE project,but i come across some error,and i do not know how to solve it?

the Error shown as below:

pastedImage_232.png

ALL the error is the same.

the Attachment is the my project.

5 Replies

1,302 Views
Daniel_Popa
NXP Employee
NXP Employee

marekstulrajter‌,

Can you help us in this matter? I do not know if there are any plans to support the demos on older IDE platforms. Perhaps such project already exists.

Thank you!

Daniel

0 Kudos
Reply

1,302 Views
Marek_NXP
NXP Employee
NXP Employee

Eden Li,

The CodeWarrior is an obsolete IDE platform and is not being supported any more. Please use for your work S32DS for power PC, version 1.2.

Your issue is being solved at the thread https://community.nxp.com/thread/45611

I consider this thread answered, further comments will be discussed in S32 community.

Best regards,

Marek

1,302 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi edenli‌,

What's the error in S32DS v1.2 ? Perhaps you should report it to S32DS S32 Design Studio Community.

Regarding the old IDE (which i honestly don't know how to use it) i seems like you need to add a define like this

SWLIBS_DEFAULT_IMPLEMENTATION=SWLIBS_DEFAULT_IMPLEMENTATION_FLT

This is how you do it in S32DS but i do not find a way to add in CW IDE.

pastedImage_2.png

Best regards,
Daniel

0 Kudos
Reply

1,302 Views
edenli
Contributor V

Hi Daniel,

About the S32 Error,i have posted it in the S32 community,but none answer me!

https://community.nxp.com/thread/456117 

0 Kudos
Reply

1,302 Views
edenli
Contributor V

Hi daniel,

Three days has passed,but my question have not been solved in the S32 community,

I import the S32 dual motor project from NXP,but has the Error 

Friend, Can you help me?

0 Kudos
Reply