while using RTCS_ping function i get wrong return code.
I checked that by putting message to debug port when i get ICMP reply message.
ICMP reply message gets printed as MCU got reply but RTCS_ping function returns timeout...
:smileyconfused:
has anyone experienced this behaviour?
已解决! 转到解答。
I've looked in mqx 4.02 source and compare it to 3.8.1
In "rtcs/source/tcpip/tcpip.c" I've noticed how timeouts are differently handled
I've also updated ping function to version from MQX 4.02
so it solved my problem...
unfortunately i do set ping_timeout every time before calling RTCS_ping
also i'm seting gpio output high at begining of ping function
and low after ping function and measure that time on scope
when i get return 0x1580 from RTCS_ping
and i'm measuring on scope wrong timeout as if function RTCS_ping immediately exited
I am using MQX 4 and the RTCS_ping returned 0 with ping_timeout changed to 0 on return - sometime I will get 0x1580 back but not very often. I think the problem might be related how it handles the timeout - it seems incorrect.
I did not dive into the code and see how it is implemented - but no surprise it not working correctly.
If you could, try to debug MQX code and help MQX guys. :smileywink:
Hi,
just to clarify things: We changed the way RTCS handles events a little in MQX 4.0.2 (because we similiar bug earlier) and further improvement will be added in MQX 4.1 (to fix another related bug). We also plan to release fix for this bug as separate patch. Thank you for effort you put in analysis of this problem and helping us in improving MQX and RTCS.
Best Regards
Karel
i left system working overnight...
total ping call's were about ~47000.
Of that number RTCS_ping timeout exceeded 200ms about ~4000 times
this is shown in histogram
I'm pinging adresses which i know doesn't exist in network so function should timeout.
so my question is.... why so much non determinism? has anyone experienced similar behaviour?
I've looked in mqx 4.02 source and compare it to 3.8.1
In "rtcs/source/tcpip/tcpip.c" I've noticed how timeouts are differently handled
I've also updated ping function to version from MQX 4.02
so it solved my problem...
seems I know the reason - the ping_timeout needs to be set every time - I do not understand why it requires a pointer and also modify the value. This does not make sense.
ping_timeout =5000; | |
ping_ret = RTCS_ping(IPData.gateway, &ping_timeout, ++pingid); |
Well, I do - but not sure it received ICMP reply or not. From the Ethereal capture YES - it should get the reply. Once it got the timeout (return 0x1580 from RTCS_ping) it seems never recover from it.