Where is the chat_client run.html from MQX + KSDK example?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where is the chat_client run.html from MQX + KSDK example?

跳至解决方案
577 次查看
lfschrickte
Contributor IV

Hi,

The updated httpsrv demo for MQX RTOS + KSDK shows an application to the new Web Socket feature and that is cool!

However, the readme file and the own http server asks the user to open a file called run.html on the chat_client folder, but neither of them is available in my files!

I also want to note that in this demo I needed to put lines to init the hardware and serial console in order to put printf to work. I've added both "hardware_init();" and "dbg_uart_init();" calls. I also had to add some files to the compilation, following the lwip examples, from /httpsrv_frdmk64f120m/utilities folder (also added "${ProjDirPath}/../../../../../../../platform/drivers/uart/common/" to the compiler includes). Is there any other right/official way to make this work?

Thank you very much!

Luiz Fernando

标签 (1)
0 项奖励
回复
1 解答
432 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached the file.

Luis

在原帖中查看解决方案

0 项奖励
回复
1 回复
433 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Find attached the file.

Luis

0 项奖励
回复